AXIS#.DBILIMIT

Description

This parameter sets the maximum amplitude of the current for dynamic braking.

Example

Setting AXIS#.DBILIMIT to 2 limits the dynamic brake current to 2 Arms.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0 to minimum of drive peak current (IPEAK) and motor peak current (AXIS#.MOTOR.IPEAK).

Default Value

Minimum of drive continuous current (ICONT) and motor continuous current (AXIS#.MOTOR.ICONT).

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.DBILIMIT 0x5000 0x7 UDINT 1000:1 - RW False
AXIS2.DBILIMIT 0x5100 0x7 UDINT 1000:1 - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen